We have had issues with the IndraDrive where end users change the communication protocol with the drive display. We solved that issue by setting P-0-0680, bit 14 to 1. I see that P-0-0680 does not exist on the ctrlX Drive, is there an equivalent parameter or any plans to add an equivalent parameter?
Locking ctrlX Drive Display
Best reply by Drives_Uwe
There are no plans to do such a simple protection of changing parameters over the panel but in the coming firmware version we will introduce a customer protection system which will allow not only to secure that somebody is changing the field bus communication type but as well other parameters, the OEM or enduser may decide.
1 reply