Default parameter of S/P parameters ctrlXdrive not correctly set Fwa 316

HEllo,

Nb: i Use drive fwa 316 and ctrlXCore RM2303

It looks like the S/P default of ctrlXDrive are not calculated based on the unit "/min" or "/sec" which is selected in the mechanical scaling.

as an example S124. default parameter = 200. I could understand the sense of this value if "/min" is choosen. 

But if "/sec" is choosen then 200 makes no sens. 

I recognised this problem because I tried to use the "MB_FixedStop" Fb with ctrlXCore and the system returns an error because S124 has a too high value.

So could you ask the dev departement to solve this issue because We will have to face probelm with customer.

Best reply by CodeShepherd

Thanks for bringing this up. Currently all default Parameter are fix values and not recalculated by loading basic parameter. See online documentation for information about the values. We will check it internally.

View original
1 reply