ctrlX Drive PROFINET communication issue

Trying to add a ctrlX drive with enough data to a Profinet master does not work. In picture one everything is ok and the profinet master finds the correct modules in the drive and profinet communication can be established.

In picture two, one 4 byte parameter is added to the drive mdt, and the master does not find the input module anymore. The profinet communication can not be established. Am I missing something or is this a feature of the system?

 

Also a question on the forum about examples for Siemens PLC has been asked and the answer was examples will be made when there is enough interest from customers. Well at least in our country unit there is interest and a lot of usage of our drives behind Siemens masters.

 

Best reply by Gruffi

Hello this is actaul a runtime bug.

We expect the new runtime in the next two weeks ( new AXS03V08-NN.02 fixed this issue).

-----------------------

General important hint for Profinet with CtrlXDrive runtime AXS03V08-NN.00:

à   Actual max. 9 parameters works as process data, not more!!

------------------------

View original
7 replies