Problem with pyusb- libusb backend not found

 

I wanted to play around with the pyusb library, but I have the impression that the library is not fully recognized.
I created a node and wanted the node to display a list of the current USB devices.
However, the problem seems to be in the backend
I've already searched the forum and tried a few things, but I still can't get the problem resolved.

 Was looking were the library is

However he cant find it while snapping

Here you can see that the problem is the backend

 

 

Here is my code

 

Snapcraft(maybe here is my fault)

Best regards

 

 

Best reply by bostroemc

Which ctrlX CORE model are you using?  I see that you have built an ARM64 snap (typ. for ctrlX CORE X3), but you have hardcoded a path with the x86_64 triplet (typ. for ctrlX CORE X7):

  

Maybe this mismatch is your problem.  

To avoid hard-coding the target triplet, one nice option is to use sysconfig.get_config_var as shown below.

View original
2 replies