Which version to select for new project, 2.6 or 3.6?

Hello,

We're going to start a new project, order new PLC's but I'm little confused about CtrlX versions. I couldn't find a clear distinction between 2.6 and 3.6 versions, other than "Release cycle". Is the latest version is 3.6, so should we start with it? Is there any limitations on 3.6 or unsupported features? Like if a tutorial explain something in 2.6 or 1.20, would it also work on 3.6? For example, we are going to use a Kassow robot, and I'm planning to use https://community.boschrexroth.com/ctrlx-automation-how-tos-qmglrz33/post/connect-kassow-robots-rc-with-ctrlx-plc-via-profinet-7mrCU4WMddc5jAP this tutorial but I'm not sure if there is any issues or not.

Because I can see 3.6 updated on 10.25 but since then 2.6 got 2 updates, one being just last month, that's why I wanted to ask.

Thank you for your support.

5 replies