ctrlX Works : Virtual control Failed to sync vcpu reg

Hello ,

ย 

ctrlX Works WRK-V-0116

When starting to run VirtualControl-1 we get the error "Failed to sync vcpu reg" and VirtualControl-1 goes to Offline .

Best reply by FooFighter

Hello,

We had the same problem on another PC, here is the solution for this PC:
On the PC there was running a software called HP-ShureClick. This is software that encupsulates some applications running in virtualized environments, and therefore the virtual cpus could not be used by INTEL HAXM.
Workaround: Start the virtual control without any hardware acceleration (is too slow)
Or: as described in https://stackoverflow.com/questions/17024538/how-do-i-fix-failed-to-sync-vcpu-reg-error

HP SureClick is a security protection program which runs "unsafe" programs in micro-VMs. It may also be called HP Wolf Security on your machine, which is the new name for it, although under the hood (e.g. folders, dialogs etc) it's still called SureClick. It may have some processes visible in Task Manager with a prefix of "Br", which stands for Bromium.
Similarly to other answers, it cannot be running at the same time as Android Emulator, as it is basically a virtual machine.
Here are some steps to disable it (not all may be required but this worked for me):
1. Right click on "HP SureClick" or "HP Wolf" in your system tray and select "Disable Threat Containment". It will pop up a dialog asking for the reason (optional), so just click OK
2. Right click on the icon again and select "Disable Malware Protection"
3. Click Start, type "services", open the Services window and set all "HP SureClick" services to disabled by right-clicking on each -> Properties -> change startup type to Disabled (for me there were 3 such services)
4. Restart the computer
After doing this, I was able to start a virtual control with INTEL HAXM Hardware Acceleration ๐Ÿ™‚

Regards,
Oliver

View original
3 replies