CtrlX PLC Enginnering (Codesys) Trace delay and lags in CtrlX Virtual Core

Hello,

our customer Cama is evaluating our CtrlX system and one of the features they liked most was the possibility to almost completely virtualize their machine cycle using the CtrlX Virtual Core, but testing it they found that sometime making the cycle trace using the PLC trace in out PLC Engineering has lags compared with the same cycle trace done on a real CtrlX Core. They asks us if there is any way, settings or something else they can use to make the robot trace on the virtual control always as it is in the real CtrlX core eliminating delays and lags in the trace result.

This is very important for then because they need to simulate their macine cycle before the real machine commissing on the floor.

Many Thanks

Giuseppe

2 replies