Hello Team,
I am making a configuration on CtrlX Configurator, please find the configuration image attached. I can see that the Mains filter size is automatically choosen, with the current configuration with XCD2323 DC bus coupled with 2 XMD0606 i get 16A mains filter, but i feel it has to be 30A mains filter.
Question 1: can we change the mains filter size in the configurator in the XCD2323 configuration or we need to add it separately by selecting the XCD2323 without filter option?
Question 2: Is my calcualtion correct or is there something I am missing?
COuld any one please help me with this?
Thank you in advance
ย