12/13/2023
Bosch Rexroth | App | System

ctrlX OS - Solutions

This system runtime app is part of the basic firmware of the ctrlX CORE control and is delivered pre-installed as standard. The system runtime app is not available separately, but can be updated individually in the engineering of the ctrlX CORE.

Each app on the ctrlX CORE must be configured according to the respective application. Travel speeds and accelerations of axes, waypoints that are to be approached by the machine, etc. everything requires application-specific settings in the app landscape. For this purpose, the Solutions App offers the option of managing all app configurations on the controller. Once created, app configurations can be saved and transferred to other devices, for example stored as backup on servers or to the control of other similar machines for easy commissioning. An important functionality when it comes to increasing standardization of machine concepts by OEMs, who create their machines as modular as possible with standardized components and the adaptation is done by the software. In such cases, the user can easily fall back on prepared app configurations that can be used flexibly from system to system. Third-party apps (apps from third-party providers) or customer-specific app configurations can also be easily integrated into the solutions app.

Support

Related Links

Curious?

You can test many apps free of charge with a virtual control system provided by ctrlX WORKS.
Just download ctrlX WORKS and follow this How-to

[link-button type="light" text="TRY IT NOW" target="_blank" href="https://community.boschrexroth.com/ctrlx-os-store-apps-oc2pqqwn/post/ctrlx-works-xOJLFLUiK4NGm5H"]

Types
ctrlX OS Apps
Categories
System

Latest published/updated articles