HI All,
I'm using the XCD drive for the first time. In my case with a keba motioncontroller. THe drives are being recognized and set in operation mode by the controller. I have given both drives an address. As soons as I activate the address check in my motioncontroller project the drives are not recogized anymore. With the XCS single axis drive this wasn't an issue. I think I need to enter a different address offset since this is a double drive but I can't find the addresses in the help or on this forum.ย