Single phase filter FN350-8-29 for XCS2-F

Is there a manual that has information about the single phase filter FN350-8-29?ย 

What is the current rating? How many XCS2-F drives can we run on a single filter?ย 

Best reply by CodeShepherd


The mains filter FN350-8-29 has a nominal current of 8A. We only did tests including one converter and one filter in combination. There have been none 1 to n tests. So we cannot say for sure if more then one drive can be connected simultaneously to one filter and will be working also in EMV compatibility.

View original
8 replies