S-0-0530, Clamping torque does not seem to work as intended

We are comissioning a machine that is using C1300 and C0600.

According to the manual the torques should be limited by this parameter when C1300 and C0600 is active:

But it isn't:

As you can se in the picture above, C1300 is active, S530 has the value of 25% but the actual torque is 40.1

Using firmware 03V12

Best reply by AndreasSwe

I tested with a Cs drive on the office, but it works with MPB20V28

The problem is that the customer are changing S92 from the PLC now so they dont see the problem anymore.

And i dont have cables to test it with a ctrlX drive.

 

 

C1300_Active.txt
550.12KB
View original
10 replies