Hello,
I have been setting and testing a demo to combine a XM22 and SMK motor with CtrlX drive XCD2. it worked for a week with cycling power on/off no issues. now somehow the CtrlX drive started setting the paramters back to factory default when recycling the powwer after I have played with sutoturing and frequency response analysis last week. I don't see there is an exchangeable battery on the drive. so I don't know why the drive parameters got back to the factory default after cycling the power. is there a parameter for setting the parameter back to factory default beside the button of load basic parameters? any help is appreciated.
Thanks,Â