Here a special question.ย
We have this RH2 cables for the one cable solution between MS2N motor and HCS01 Drive. (Encoder is 15pole sub-D)
Then we have this RHB2 cable for MS2N and ctrlX drive (Encoder is this small black connector)
Do we also have a Hybrid cable for MS2N on ctrlX drive to connect to the EC encoder interface. (Encoder is 15 pole Sub-D)
I need this back connector for the power and Sub-D for the encoder.ย Do we have that, or should I order the RH2cable with a separate black power connection ? And to be sure, the black encoder cable should be long enough to reacht the EC encoder interface on the Drive, but as I can see with Indradrive this should be fine.ย
ย