MS2N hybride cable for EC interface on ctrlX Drive

Here a special question.ย 

We have this RH2 cables for the one cable solution between MS2N motor and HCS01 Drive. (Encoder is 15pole sub-D)

Then we have this RHB2 cable for MS2N and ctrlX drive (Encoder is this small black connector)

Do we also have a Hybrid cable for MS2N on ctrlX drive to connect to the EC encoder interface. (Encoder is 15 pole Sub-D)

I need this back connector for the power and Sub-D for the encoder.ย  Do we have that, or should I order the RH2cable with a separate black power connection ? And to be sure, the black encoder cable should be long enough to reacht the EC encoder interface on the Drive, but as I can see with Indradrive this should be fine.ย 

ย 

Best reply by Drives_Uwe

MS2N motors with AcuroLink encoder have to be plugged into XG20 at ctrlX DRIVE. The multi-encoder connection at XG21 is not suitable.

Therefor the cable must be looking like RHB2.

View original
1 reply