ML3 linear motor on Ctlrx Drive?

Does the ctrlx drive can handle the ML3 linearmotors? If yes, which cables are good?

Best reply by Drives_Uwe

Yes, linear motors ML3 can be controlled by ctrlX DRIVE. Be aware that the encoder (linear scale or similar) matches the possibilities given at the "EC" encoder interface. A good choice would be to use Bosch Rexroth absolute integrated measuring system IMS-A with combined 1Vpp + Hiperface signals, where the linear scale is right built into the carriage guides.

Ready-made cables are not possible to order, yet. But simply use the ready-made cables for IndraDrive Cs and just exchange the connectors on the drive side.

View original
2 replies