Backup options using panel

While using the panel to back up the drive, there are three options available: Snapshot, Device Replacement, and Commission. What are the differences between them? Thank you.

Panel firmware: FWA-XD1-PAN-V-0116.02

Best reply by Jamie

The Snapshot option is for saving all parameters to look at later on (drive parameter S-0-0017).  Commision is for backing up all operation data (S-0-0192) and Device firmware.  This is useful for serial commissioning of devices.  Device replacemnt backs up operation data, firmware, and retain data (p-0-0195) in case you have to replace a specific device.  

See the image below for a breakdown chart:

 

View original
1 reply