Hello,
in the GET "typeplate" call to the System REST API, the response body between V01.16 and V01.18 has changed.
Response body in V01.16:
{
"typePlateType": "ctrlXCORE",
"serialNumber": "xxxxxxxxxxx",
"materialIndex": "AB1",
"materialNumber": "R9114xxxx",
"typeCode": "COREX-C-X3-11-ANNN-21.01-01RS-NN-NN"
}Â
Response body in V01.18:
{
"typePlateType": "ctrlXCORE",
"serialNumber": "xxxxxxxxxxx",
"materialIndex": "AB1",
"typeCode": "COREX-C-X3-11-ANNN-21.01-01RS-NN-NN",
"hardwareRevision": "cx_m4_a"
}REST API URL used on both images: /system/api/v1/typeplate
Is this change intended or an bug?
If the change is permanent, where is the materialNumber available via the REST API?
Thanks