Hello,
I'm trying to install node-red-node-email in the Node-Red for ctrlX.
But there is always an error. The protocol is down below.
I also tried to run the px.exe, set up the firewall entrance rules and restart the ctrlX. But the error still scours.
Attached the screenshots of the Settings.
The browser is running on a vMware and connected in a local network with the ctrlX. The vMWare have also a connection to the internet.
Node Red protocol:
Â
-----------------------------------------------------------
2023-02-07T12:04:35.163Z Installieren : node-red-node-email 1.18.4
2023-02-07T13:04:07.002Z npm install --no-audit --no-update-notifier --no-fund --save --save-prefix=~ --production --engine-strict [email protected]
2023-02-07T13:05:21.516Z [err] npm
2023-02-07T13:05:21.518Z [err]
2023-02-07T13:05:21.519Z [err] ERR!
2023-02-07T13:05:21.519Z [err]
2023-02-07T13:05:21.520Z [err] code
2023-02-07T13:05:21.520Z [err] ECONNREFUSED
2023-02-07T13:05:21.522Z [err] npm
2023-02-07T13:05:21.522Z [err]
2023-02-07T13:05:21.523Z [err] ERR!
2023-02-07T13:05:21.523Z [err]
2023-02-07T13:05:21.523Z [err] errno
2023-02-07T13:05:21.524Z [err] ECONNREFUSED
2023-02-07T13:05:21.582Z [err] npm ERR!
2023-02-07T13:05:21.582Z [err] FetchError: request to https://registry.npmjs.org/node-red-node-email failed, reason: connect ECONNREFUSED 192.168.100.80:3128
2023-02-07T13:05:21.582Z [err] npm ERR! at ClientRequest.<anonymous> (/snap/ctrlx-node-red/327/lib/node_modules/npm/node_modules/node-fetch-npm/src/index.js:68:14)
2023-02-07T13:05:21.582Z [err] npm ERR! at ClientRequest.emit (events.js:400:28)
2023-02-07T13:05:21.582Z [err] npm ERR! at onerror (/snap/ctrlx-node-red/327/lib/node_modules/npm/node_modules/agent-base/index.js:101:9)
2023-02-07T13:05:21.582Z [err] npm
2023-02-07T13:05:21.583Z [err] ERR! at callbackError (/snap/ctrlx-node-red/327/lib/node_modules/npm/node_modules/agent-base/index.js:123:5)
2023-02-07T13:05:21.583Z [err] npm ERR! at processTicksAndRejections (internal/process/task_queues.js:95:5)
2023-02-07T13:05:21.583Z [err] npm
2023-02-07T13:05:21.583Z [err] ERR! FetchError: request to https://registry.npmjs.org/node-red-node-email failed, reason: connect ECONNREFUSED 192.168.100.80:3128
2023-02-07T13:05:21.583Z [err] npm ERR!
2023-02-07T13:05:21.583Z [err] at ClientRequest.<anonymous> (/snap/ctrlx-node-red/327/lib/node_modules/npm/node_modules/node-fetch-npm/src/index.js:68:14)
2023-02-07T13:05:21.583Z [err] npm ERR!
2023-02-07T13:05:21.583Z [err] at ClientRequest.emit (events.js:400:28)
2023-02-07T13:05:21.583Z [err] npm ERR! at onerror (/snap/ctrlx-node-red/327/lib/node_modules/npm/node_modules/agent-base/index.js:101:9)
2023-02-07T13:05:21.584Z [err] npm ERR!
2023-02-07T13:05:21.584Z [err] at callbackError (/snap/ctrlx-node-red/327/lib/node_modules/npm/node_modules/agent-base/index.js:123:5)
2023-02-07T13:05:21.584Z [err] npm ERR! at processTicksAndRejections (internal/process/task_queues.js:95:5) {
2023-02-07T13:05:21.584Z [err] npm ERR!
2023-02-07T13:05:21.584Z [err] type: 'system',
2023-02-07T13:05:21.584Z [err] npm ERR! errno: 'ECONNREFUSED',
2023-02-07T13:05:21.584Z [err] npm ERR! code: 'ECONNREFUSED'
2023-02-07T13:05:21.585Z [err] npm ERR!
2023-02-07T13:05:21.585Z [err] }
2023-02-07T13:05:21.585Z [err] npm
2023-02-07T13:05:21.585Z [err] ERR!
2023-02-07T13:05:21.585Z [err] npm
2023-02-07T13:05:21.585Z [err] ERR! If you are behind a proxy, please make sure that the
2023-02-07T13:05:21.585Z [err] npm ERR!
2023-02-07T13:05:21.586Z [err] 'proxy' config is set properly. See: 'npm help config'
2023-02-07T13:05:21.605Z [err]
2023-02-07T13:05:21.606Z [err] npm ERR! A complete log of this run can be found in:
2023-02-07T13:05:21.606Z [err] npm ERR! /root/snap/ctrlx-node-red/327/.npm/_logs/2023-02-07T13_05_21_589Z-debug.log
2023-02-07T13:05:21.640Z rc=1