How to avoid appData misfitting problems when updating a ctrlX CORE to v1.10

How can a customer avoid problems with appData misfitting when updating a ctrlX CORE to the release RM21.07 (v1.10)?

Best reply by CodeWasi

Setting up a new ctrlX COREvirtual is based on a image and scheduler config which does not fit to your setup by default.

Assuming e.g. the motion app was installed and swichting to RUN-Mode is not possible you may struggle because of misfitting configs.

Either you can configure the avialbable "app-callables" manually or you Reset the configuration by following button under Manage app data

Since the process gets modifcated with the next release we recommend to just click ones the reset-button in the configuation

Missfitting Setups - for instance: the installed motion.app is not represented.
Booting the motion will never lead to run, since the callable is not called....

After the Reset:

In case the reset is performed - dont care about the intergration:

Manually setup as an alternative in general:

Individual setup ot the callable inside the scheduler config. started with +sign

View original
1 reply