CtrlX core X3 profinet device transition in safe-op

we got a demo of CtrlX Core X3 with profinet slave ports at xf-23 and xf24. the profinet device app and other apps (version 1.16)were installed and licensed. after having XF23 port configured as profinet device and running the transition status is always at Safe-OP mode. 

when checking the scheduler it shows operating.

since the CtrlX I/Os have not been installed yet the Ethercat Master has an error "Topology not OK"

this is the first time to test X3. does the Ethercat master error affect the profinet status?

then I set up a XM22 as profinet master and loaded the device data file. the master can have the device scanned. after having the settings applied in the project and downloaded it showed module not found.  

from that I can guess the issue is from the CtrlX core X3, but after having most settings checked I haven't seen where to change the profinet settings and how to fix it. let me know if I have missed any settings. 

your help will be appreciated.

 

 

 

Best reply by CodeShepherd

Release of the ctrlX Profinet Device App is now planned for KW3 2023.

View original
8 replies