Hi,
I have a FESTO CPX over EhterCAT with valves VMPA2 and electrical inputs CPX-AP-A-8DI.
The ctrlX IO, ESI file and datalayer configuration look OK. I can control the valves. However, i cannot see the state of the inputs in ctrlX Eng and even in ctrlX IO, nor in the datalayer. I can only see the actual values in the CoE.
LEDs on the FESTO module = TRUE
CoE
0x6010:01= TRUErealtime_data/.../Inputs.Input_0= FALSEctrlX IO variable = FALSE
ctrlX Eng = FALSE
The mapping of TxPDO looks correct. The process data are activated. I don't see what's wrong.
Thanks for your help.
Thomas