12/15/2023
REST, API, JSON, YARC

Using REST API of ctrlX OS

Overview

This blog will show you how to use the REST API of a ctrlX OS device (e.g. ctrlX CORE or a ctrlX COREvirtual) to read out data of the ctrlX Data Layer. With this interface the control can also be configured and axis be commanded (see hints and the end).

Preparation

  • A ctrlX OS device has to be connected to the network

  • An installation of the ctrlX MOTION app is needed for the following examples

  • Installation of a REST client on engineering PC is expected. In this Example Google Chrome extension YARC! is used

  • Make sure the browser is allowed to connect to the control via https by trusting its certificate or install corresponding web certificate and key (See "How to make secure HTTPS connection with ctrlX OS Web Server").

    Trust certificate of ctrlX OS
  • Optional: Installation of ctrlX WORKS. Please have a look at the corresponding documentation or video to see how to do this.

  • Hint:
    read = GET, write = PUT, create = POST, delete = DELETE.

Using REST (Representational State Transfer) API (Application Programming Interface)

1. Check connection

Check the connection to your ctrlX OS device with your network folder of windows or use our tool ctrlX WORKS. There all controls connected to your PC and their IPs are shown.

2. Authorize

The system is secure by design, so to get access to the control you will always have to authorize your requests with a security token.

To get it send an https POST request to the authorization server of the ctrlX OS (https://192.168.1.1/identity-manager/api/v1/auth/token). The payload has to be a permitted user and a password written as a JSON (JavaScript Object Notation) object. The standard ones are “boschrexroth” ({"name":"boschrexroth","password":"boschrexroth"}). 

The response will show the number 201 that means successfully created and includes a JSON object with the token of the type bearer.

REST API - get authorization token via YARC

3. Use token

Get access to all data of the ctrlX OS by adding the token to the request header as "Authorization" changed to the format

"Bearer xxxxx..."

 

4. METADATA

To get to know which command can be used on which ctrlX Data Layer node additional information can be read out via a GET request of the type metadata. Exemplary the "axs" node of motion (https://192.168.1.1/automation/api/v1/motion/axs?type=metadata). Response is a JSON object including all information. Additionally the “Content-Type” “application/json” has to be added to the request header to tell the server how the sent data should be interpreted.

REST API - browse node via YARC


5. BROWSE

A browse request can be send at any node of the ctrlX Data Layer to get a list of sub nodes.

To read all actual known axes in the ctrlX MOTION system by sending an https GET request of the type browse to the axes area of the motion (https://192.168.1.1/automation/api/v1/motion/axs?type=browse) to get to know which ones are available. Response is a JSON object including the type "arstring" and the list of axis names.

REST API - Send Browse Request


6. GET

Now send an https GET request to read out the actual values of the axis (https://192.168.1.1/automation/api/v1/motion/axs/Axis_1/state/values/actual/) found by browsing. Here the response contains a JSON object with all the data included.

REST API - get axis value via YARC


7. PUT

Now send an https PUT request to write a limit of the axis found by browsing (https://192.168.1.1/automation/api/v1/motion/axs/Axis_1/cfg/lim/pos-min). As payload we have to hand over a JSON object with the data type and the value.

REST API - write axis limit via YARC

7.1 Bulk requests

Now send an https PUT request to issue e.g. a bulk read to get several system information via one request (https://192.168.1.1/automation/api/v2/bulk?type=read). As payload hand over a JSON object with key value pairs of the expected data type and the node path on the ctrlX Data Layer.

REST API - bulk request via YARC

8. POST

Now send an https POST request to create new axis "Axis_new" (https://192.168.1.1/automation/api/v1/motion/axs). ctrlX MOTION needs to be in configuration state. As payload we have to hand over a JSON object with the data type and the value.

REST API - create axis via YARC

9. DELETE

Send an https DELETE request to the path https://192.168.1.1/automation/api/v1/motion/axs/Axis_new to remove an axis "Axis_new". ctrlX MOTION needs to be in configuration state.

REST API - remove axis via YARC

Notes

  • When using a ctrlX COREvirtual in port forwarding mode the address will change to https://localhost:PORT/... (PORT in standard is 8443)

  • REST = Representational State Transfer
    is a software architectural style that defines a set of constraints to be used for creating Web services.

  • API = Application Programming Interface
    is a computing interface to a software component or a system, that defines how other components or systems can use it.

  • JSON = JavaScript Object Notation
    is an open standard file format, and data interchange format, that uses human-readable text to store and transmit data.

  • The old version of the REST API is using v1.0 and the new one v1 in the corresponding links.

  • The validity time of the authorization token can be set via ctrlX OS web UI in the "Users & Permissions" area under "Session Policies". They will automatically expire with a control reboot.

  • A list of ctrlX OS APIs can be found via its web UI or via addresshttps://<IP of device>/device-dashboard/api-reference 

    ctrlX CORE web UI - API reference and swagger

  • Any standard browser is also using the REST API. With the developer tools (open with "F12"), the used commands can be visualized.

    REST API in browser development tools

Related links

10
yarc_favorites.zip
2.5KB
Types
How-to
Example
Products
IOT
Controls
Markets
Manufacturing
Assembly Lines
Building Automation
Logistic
Packaging
Printing
Production Machines
Robotics
Semicon & Electronics