04/04/2024

Setup a SMC JXCE Controller with EtherCAT

This how-to describes the integration of a SMC EtherCAT JXCE controller into the ctrlX OS environment. It shows how to set up the communication.

Requirements 

Hardware

  • ctrlX CORE
  • SMC EtherCAT JXCE controller (e.g. JXCE1) 


Software


Step-by-Step guide

Step 1: Start a new EtherCAT Master project 

  • Open ctrlX CORE user interface in your browser. 

 

crtlX OS user interface

  • Add EtherCat master by clicking “+” in EtherCAT configuration. 

crtlX EtherCat configuration

  • Add EtherCAT Master and give it a name.

crtlX EtherCat Master

  • Open ctrlX I/O Engineering by clicking on the Name of the Master system.

crtlX EtherCat Master

  • Open new „crtlX CORE I/O“ project and give it a name.

ctrlX I/O Engineering

Step 2: Install the JXCE device description

SMC Download page

  • Install the device description in the “Device Repository” chapter in the software.

ctrlX device repository

Step 3: JXCE device configuration in the project

  • Add device to EtherCat Master by right-click in the device tree on ethercatmaster.

ctrlX add device

  • Choose the relevant device description for your device from device catalog and add it.

ctrlX SMC device catalogue

  • The JXCE controller is now installed and available.

ctrlX SMC device ready

Related Links 


The Company 

Founded in April 1959 in Tokyo, Japan, SMC Corporation today employs over 21,600 talented employees in over 80 countries worldwide. The SMC Group entered the pneumatics market back in 1959 and, since then, we have evolved, together with our customers’ requirements, to build a comprehensive automated control equipment portfolio. 12,000 basic models with over 700,000 variations, designed to provide you with greater competitiveness.

Types
How-to