10/29/2024

Import EtherCAT IO realtime data offline into ctrlX PLC Engineering

Content

This guide shows how you can import EtherCAT IO real-time data into ctrlX PLC Engineering without a connection to a ctrlX CORE.

ctrlX PLC and ctrlX IO Engineering - IO configuration

Requirements

  • ctrlX WORKS needs to be installed
    • ctrlX PLC Engineering
    • ctrlX IO Engineering

Explanation

Case 1: Download from ctrlX CORE

After a download from the ctrlX IO Engineering to a ctrlX CORE the EtherCAT configuration file is located in active configuration (app data) and can be downloaded from there.

ctrlX CORE web UI - EtherCAT configuration file

Case 2: Export from ctrlX IO Engineering

The EtherCAT configuration file can be exported from the ctrlX IO Engineering via right clicking the EtherCat master and choosing "Saving EtherCAT Configuration...".

ctrlX IO Engineering - saving EtherCAT master configuration

If not visible in the engineering it needs to be added by hand.

ctrlX IO Engineering - show save EtherCAT menu

Import real-time data in ctrlX PLC Engineering

When EtherCAT master configuration file is available it can easily be implemented into the ctrlX PLC Engineering via the real-time data node in the "Devices" tree.

ctrlX PLC Engineering - import EtherCAT realtime data from file

Related information

4
Types
How-to
Products
Controls
IO
PLC