12/04/2023
How-to | ctrlX OS | ctrlX CORE | ctrlX WORKS

How to generate a system report and switch on additional traces

Content

This article shows how to generate a system report in the control ctrlX OS and the software tool ctrlX WORKS and how to switch on additional traces in the ctrlX OS via the data layer.

Requirements

Connection to a ctrlX CORE device, ctrlX OS or ctrlX WORKS installed on a PC

Explanation

ctrlX OS 1.12

Via the about area in ctrlX OS web UI:

ctrlX CORE web UI - generate system report 1.12

ctrlX OS ≥ 1.20

Via "?" symbol on the right top in your crlX OS web UI:

ctrlX CORE web UI - generate system report x 1.20

Additional traces on ctrlX OS

Installed apps can have internal traces for deeper analysis by the developers. These can be published into the diagnostic logbook of the ctrlX OS.
If asked to, activating is done via the data layer by writing three times true (or 1) for switching on messages, warnings and errors. Beware that activating traces can add a lot of additional messages and  postpone other ones, so the standard setting should be deactivated.

e.g. to the paths for:

  • general motion purposes "trace/rexroth-automationcore/units/motion/core"

  • switching up problems of the axisprofile "trace/rexroth-automationcore/units/comm/axisprofile"

  • switching state problems of the EtherCat master "trace/rexroth-automationcore/units/comm/ethercat"

ctrlX CORE web UI - data layer viewer - Ethercat master traces

If this settings needs to be persistent an save (via create) needs to be executed via the ".../admin/cfg/save" node sending payload {"configurationPath": "", "id": "", "phase": "save"}:

ctrlX CORE web UI - data layer viewer - save setting

Note: By setting values in a top node (e.g. units/comm) all subsequent nodes (e.g. units/comm/ethercat) are also set.

ctrlX WORKS 1.12

Via the about area in ctrlX WORKS UI:

ctrlX WORKS - generate system report 1.12

ctrlX WORKS ≥ 1.20

Via "?" symbol on the right top in your crlX WORKS UI:

ctrlX WORKS - generate system report x 1.20

Related information

1
Types
How-to
Products
Controls