09/29/2021

Do autotuning of regulation loops with ctrlX DRIVE

If you want to download a step-by-step procedure use the zip-File in the attachment.

Pre-requisite: "Start easy startup mode".

1. Autotuning in standard mode

Select menu: Automatic setting of position/velocity control loop. Then select the method "Optimization with axis motion (in AF)".



Best use the "Absolute travel limits (X1 : X2). Key in the intended positions. In here 10 mm and 50 mm are used.





Now the auto-tuning process will take place. In the end the new optimzed parameters are shown "Value (after)". If pressing the button "Finish" the new obtained values are taken over.

2. Autotuning in Expert mode

Alternatively the so called Expert mode can be used.



A new menu is showing up. We recommend to set the following parameters:

 

Press button "Start optimization".



Once again the optimized value are shown in "Value (after). By pressing button "Finish" the values are taken over.

 

Related Links

Autotuning of regulation loops.zip
675.17KB
Types
How-to
Products
Drives