11/11/2024
Selmo | How-to | Nov 11, 2024

Demo Conveyor Belt with Selmo

A box is transported from A to B via two conveyor belts.
 

Functional Description

A crate is to be transported via a conveyor belt. The crate is to be transported from A to B via two conveyor belts. After pressing the start button, the crate is to be placed on the conveyor belt. By occupying the sensor (B1), conveyor belt 1 is started and the crate is transported to the next sensor (B2). After occupying the sensor (B2), conveyor belt 2 is started and the crate is conveyed to the next sensor (B3). After leaving the sensor (B3), the crate lands on the ramp and the system switches off.

In/Output assignment

The in- and outputs of the model are assigned as follows (the designation input or output refers to the connected controller):

Input Nr.NameFactory I/O Variable nameTypSpecification1S1I_StartBOOLStart button (NO)2

B1

I_Sensor_1BOOLSensor B1 (light barrier NC)3B2I_Sensor_2BOOLSensor B2 (light barrier NC)4B3I_Sensor_3BOOLSensor B3 (light barrier NC)

 

Output Nr.NameFactory I/O Variable nameTypSpecification1O1O_Conveyor_1_ONBOOLConveyor belt entrance on2O2O_Conveyor_2_ONBOOLConveyor belt exit on3O3O_Load_PackageBOOLLoad package

 

How-to

Support

 Forum ctrlX World Topics
 [email protected] 1)
 Selmo Helpcenter

Related Links


The Company

Selmo Technology GmbH rethinks machine programming and reduces complexity for the programmer. We offer an alternative for manual programming of processes and can translate the process model directly into a PLC program through our algorithm. The Selmo Solution can be learned and applied quickly and easily and immediately creates a standardisation of PLC programming.

FOR SOFTWARE THAT NEVER LETS YOU DOWN


1) Note on data protection
The email is sent directly to the partner company! This company is responsible for the processing of the data contained. Please read their data protection information before sending this email! 
Bosch Rexroth is not responsible for the use of the partner company's support.

Specification Conveyor Belt EN.pdf
521.82KB
Conveyor_V2023_1.zip
24.15MB
Types
Example
Markets
Packaging