Hello
I am using the ctrlX Core as Modbus Client. Writing and Reading from the Modbus server does generally work, so i guess the configuration is correct. After an uncertain period of time (a few minutes up to about a hour) fails the writing operation.
The write access is done with the PLC function block IL_ModBusTCPWriteMultipleRegisters from library CXA_MODBUSTCP version 1.20.0.0. The ErrorIdent could not be found in the documentation and is: Table: CXA_TABLE, Additional1: 16#0A0F1850, Additional2: 16#0C230006
Does anyone have more information about this error code?
Thank You