I am wanting to interface a Beckwith M-3410A protection relay to the CtrlX core. We are already using the Modbus TCP app. Can I use a modbus gateway to convert RTU to TCP in order to communicate with the core? Is it possible to use the USB-C port on the core for this, or must I use an ethernet port (XF10 and/or XF51)?
Modbus gateway to convert RTU to TCP to interface with core
Best reply by CodeShepherd
There are different ways to directly connect Modbus RTU to the ctrlX CORE.
- Using our S20-RS-UNI module. See this post.
- Using Node-RED and an adapter. See this post.
- Using the Bosch - DeviceBridge to directly bring the data to the data layer.
1 reply