I am trying to establish connection to Elmo Drive via EoE, but it is not working.
EtherCAT Master:
Enabled IP Forwarding:
Command Prompt ping successful:
Elmo Application Studio:
Anyone have success connecting into Elmo drive?
Warmest regards,
Best reply by CodeWasi
Hello , checked the setup of EOE with a HarmonicDrive und a ctrlX. Enable the IP Forwarding on XF10 and EoE like you show in your screens. ctrlX-IO Setup done like you did. Please consider to test the EAS connection running ECAT_EoE_TCP/IP protocol. I am not that familiar with the dos and donts... but the EAS relies on cyclic and fast communication with ms. I assume your ECAT operates as well with 2ms, right? I did not find a adjustment for the Mailbox-settings and left it default. Find the figures below:
EAS : File/Settings:
EOE Routing (consider to 255.255.255.0)
Destination: _._._.0 Network-number; Gateway: Â IPctrlX Â Â
Target the EAS wants to communicate: Â
Check the IP Forwarding.
Â
If the setup will not succeed - please consider return with Elmo-Drive-FW-infos.