Hello,
I have an OPC UA Server with the following server settings:
I can connect to the Server with UAExpert without any problems.
But when I try to use the Rexroth OPC UA Client App (running on a ctrlX-Core-virtual) an error occurs:
I can add the Server in the opcuaclient-node with the "create" method. But when I try to use the "connect" method I get: "The method has no arguments" "Call failed with status 'Bad'"
My session-configuration is:
In the logbook on my ctrlX-Core-virtual I get the following:
How can I resolve that problem?
Thanks in advance!