I've created an HTML5 control for ctrlX PLC Engineering (WebVisu) using the HTML5 Control Editor included in ctrlX WORKS 1.18. If I try to open the control (i.e. the *.html5control.xml file) in the HTML5 Control Editor included in ctrlX WORKS 1.20, I get the following exception:
Note that in the former case, ctrlX PLC Engineering is based on CODESYS 3.5.18.30, whereas in the later case ctrlX PLC Engineering is based on CODESYS 3.5.19.10. Â
Is this a known issue? What I'm seeing is identical to what was reported in this thread.
Unrelated question:Â Is it possible to suppress the console entries that are logged automatically whenever the prototype functions are called?