WebIQ runtime gets unreachable

Hi!

I use ctrlx Core X3 with firmware: 18, and WebIQ app 2.13 in my system.

Unfortunately i have the following experience. If my machines are switched on continously for ~1 day or more, then my webIQ project usually stops working. Unfortunately at this case the web iq runtime is also not reachable on the ctrlX (host:10123). After restarting ctrlX core everything starts working perfectly, and the web iq runtime page gets also available.

After reboot of two machines I downloaded the logfiles. So these were created after the mentioned bug, and after restart.

I attached them.

Thank you in advance!

Best reply by HmiGuide

WebIQ 2.14 is now alvailable in the store. Please give here a feedback, if your issue is solved or not.

Feedback from customer: Problem fixed in 2.14

View original
BalancerWebIQ_log.log
42.08KB
coffeMachineWebIQ_log.log
3.12MB
4 replies