Update HMI from 2.12 to 2.13

I updated WebIQ server and designer from 2.12 to 2.13. The thing is that I need my projects from 2.12 to be update to 2.13. When I try to start it from my CtrlX WebIQ runtime manager, I have the message "projet version not compatible... see WebIQ designer manual chapter project list". In the manual, chapter project list, the only thing I see about uptdating project is in 2.1 -> point 3 (see screenshot below), I follow the steps, uptdate of the visual package is done. but when i publish the project to save the update, it does not work, the screen shows "publishing HMI project" and never changes (see screenshot below), I have waited half an hour, and still nothing has change. I have to restart the CtrlX.

do you knwo how to fix it ? or could you update my projects and send it me back ?

PS : I made it with 2 different projects and 2 different CtrlX... same result.

Thank's in advance,

ย 

ย 

Best reply by joelphilippage

We got this working on our PLC by doing a reset and then reloading everything. Uninstalling and re-installing just the app did not work so something else in the data must cause the error.

View original
1
17 replies