Local Connect is in Runtime Mode, WebIQ Designer cannot be used. Error

Hello everyone,

ย 

I wanted to connect with the WebIQ Server from my core over the WebIQ Designer with the extension " --ws-host=10.52.152.57 --ws-port=10123", resulting in the error message below:

I disabled the running HMI on the core server using the remote runtime manager and also stopped the local server on my PC without success.

ย 

I'm thankful for every suggestion.

Felix

Best reply by felX_CORE

The Message occured because of the unfinished licencing.

With the new WebIQ Server App 2.9.2 and my installed license it works like charm.

View original
1 reply