Hello everyone,
I created in the WebIQ Designer a hmi and it is localy running also and sucessful connectet to the ctrlX core via opc ua.
Now I want upload the designed HMI to the WebIQ app which is installed also in the ctrlX Core.
But it seems the connection from WebIQ designer dosn't establish. First try was the remotemangaer from WebIQ Designer, it search unendless for the ctrlX, and the second way was startig WebIQ Designer with parameters in the command promt (Â "C:\Program Files (x86)\WebIQ\Designer\webiq-designer.exe" --ws-host=192.168.1.1 --ws-port=10123 ).
The Results you will see in the attachment.
May I have to do more settings in ctrlX?
Thanks for answers in advanced, Matthias