Hi together,
One of our customer is testing now WebIQ to decide if it's convenient for their applications. He has the questions below;
1. How is it possible to specify the color of the image in a Widget Button. (e.g. green enabled, black disabled)
2. How to change the image in a button dynamically with a PLC variable?
3. How to change the displayed color when a button or input widget is locked?
4. Layout: How is it possible to design different layouts?
5. Dialogbox:
5.1 How is it possible to make the Header invisible?
5.2 Can scripts be used to open the dialog and then make different settings depending on a variable?
E.g. by type=0, then Text with Value1 and Errofeld(Label) visible
by type 1, then Text with Value2 and and Errofeld(Label) visible
6. OPC-UA: How to open an own messagebox dialog when changing the value of an OPC-UA variable "Error"? Or start an action o a value change, or describe local variables?
7. Are there detailed documents explaining what we can do with commands in "scripts" and "CSSs"?
Kind Regards,
Emrah Emre