Different WebIQ Questions - Widgets, buttons, layout, OPC-UA and scripts

Hi together,

One of our customer is testing now WebIQ to decide if it's convenient for their applications. He has the questions below;

1. How is it possible to specify the color of the image in a Widget Button. (e.g. green enabled, black disabled)

2. How to change the image in a button dynamically with a PLC variable?

3. How to change the displayed color when a button or input widget is locked?

4. Layout: How is it possible to design different layouts?

5. Dialogbox:

5.1 How is it possible to make the Header invisible?

5.2 Can scripts be used to open the dialog and then make different settings depending on a variable?

E.g. by type=0, then Text with Value1 and Errofeld(Label) visible

by type 1, then Text with Value2 and and Errofeld(Label) visible

6. OPC-UA: How to open an own messagebox dialog when changing the value of an OPC-UA variable "Error"? Or start an action o a value change, or describe local variables?

7. Are there detailed documents explaining what we can do with commands in "scripts" and "CSSs"?

Kind Regards,

Emrah Emre

Best reply by webiq-sk

I just noticed you were probably talking about the dialog header and how to hide it. My answer is the same here: it can all be done with CSS.

I have attached another demo that includes hiding the dialog box header.

icon_changing_button2.zip
4.73MB
View original
4 replies