Hello,
we have a WebIQ server with two different projects that are HMIs for the same machine, but with a different focus. One is more a viewer, while the other one is rather to control it. (But it's more than just about access rights to individual controls)
We do have 7 licenses for the server and now would like to make sure that the "control" project has always at least one license available, not matter how many clients are connected to the "viewer" project.
I found this post:
That seems to address my question. It say's it's not possible. But the post is 2 years old, so I thought it's okay to ask again. Is there a way to do that?
If there is no direct way, the post above mentions a way to count the connected clients. Is there maybe a workaround from inside the project to count the connected clients and deny further connections from there. Or even just disconnect the oldest or a random client?
Any idea is appreciate!
We work with WebIQ version 2.16.4