Hi,sir
I had developed the motion application SDK in ctrlX v1.14, and I used several functions from motion extension library like below, however, I can not find the related or similar library in v2.06, what happened to these library?
I need to use these library functions to change and read the axis and kinematics parameter like position/velocity/acceleration limitation and motion units, and so on.
#include "motion/core/extension/i_axs_cfg.h"
#include "motion/core/extension/i_kin_cfg.h"
#include "motion/core/extension/i_obj.h"
#include "motion/core/extension/i_obj_axs.h"
#include "motion/core/extension/i_obj_kin.h"
#include "motion.lib.jobs/motion/jobs/defines/cmd_defs.h"As well as the ethercat master library in V1.14 is missing in V2.06, I need this library to read and write directly from ethercat master to slave driver;
#include "comm.ethercat.master/comm/ethercat/master/fbs/parameter_generated.h"