Hi,
I'm creating a snap for a 3rd party application. This application refuses to run as root. If the application detects it's running with root permissions, it will terminate, thus the application must be executed with unpriviledged user permission within the snap context.
There is a trick how to switch from the default root user to unpriviledged user called snap_daemon inside the snap context: https://snapcraft.io/docs/system-usernames
Now the application accepts to run, but the problem is access to system resource. Snap_daemon does not have permission to bind TCP server socket for listening incoming connections (the port number is outsided of restricted range >1024).
Is there a way allow network bind for unpriviledged user?
Normal application with normal root user would only need 'plugs: network_bind' definition in snapcraft.yaml. For clarity: the problem is not related to permissions of the snap, but permissions of the application inside the snap.
Here are selected relevant parts of my snapcraft.yaml:
system-usernames:
  snap_daemon: shared
apps:
  myapp:
    command: launcher.sh
    plugs: [network, network_bind]
Â