ctrlX Core OPC UA Pub Sub to MTX

Is it possible to use ctrlX with OPC UA Pub Sub to talk to the MTX OPC UA server? 

I have customer who is planning to use a ctrlX core as a gateway from MTX to an EtherCat device. 

I read this post about ctrlX to ctrlX communications. Solved: Communication between ctrlX core's (boschrexroth.com)

However, there I can't tell if Pub Sub will work with MTX. 

 

Best reply by NoRisk4Project

The MTX system only supports OPC UA server-client. OPC UA PubSub is not implemented inside the older controls like CMLx5 or XM.

In theory you can connect a MTX with a ctrlX CORE via PLC network variables or OPC UA server-client (both NRT).
Or you can use ProfiNet to communicate between a MTX and the ctrlX CORE to connect to the EtherCAT device.

But if you just want to connect a EtherCAT device to a MTX, why you don’t use a SERCOS/EtherCAT-Bridge?

 

 

View original
3 replies