Issue Opening ctrlX PLC Engineering V1.20

Hello,

When I attempt to open ctrlX PLC Engineering V1.20 the icon shows in the task bar, but I can't interact with the application at all. I don't receive any error message when opening the software. This behavior is the same whether I open it from the Windows menu or by double clicking on a project file. I've upgraded from V1.20.2 to 1.20.4, repaired, uninstalled/reinstalled and power cycled my PC. I have no issue opening IO or Drive Engineering and I can also open PLC Engineering in V1.18.2.

The software worked initially. The behavior seemed to start after I was logged into a ctrlX Core PLC application for some period of time. The program wasn't responding and after restarting once I've been unable to work with it since.

I'm running on a VirtualBox VM.

Any suggestions would be appreciated, thank you.

Best reply by CodeShepherd

Could you please check this thread for a possible solution or send a screenshot how it looks like on your PC after starting.

View original
2 replies