ctrlX WORKS installation via command line

Hello,

is it possible to install ctrlX WORKS via command line ?ย  I mean an automatic installation on some PCs with a command so that the IT-admin has no to much to do with that.

Best reply by FooFighter

Hello st_ctrlX_user,

yes, the setup supports the following parameters:
ctrlx-works-1.18.2.exe /Path="{installFolder}" /Mode={mode} /Silent=yes

  • installFolder is the folder to install the product (must be empty for new installation) or direct to an installation folder in case of an update installation
  • mode is either "Install" or "Update"
  • Silent either yes or no

Regards,

Oliver

ย 

View original
1 reply