Hello,
I have 3 points:
1. When I want to update one ore more Apps on a ctrlX CORE through the Device Portal, it is not possible due to the ctrlX CORE isn't in "Service"-Mode. But what sense makes the Device Portal, if I need to access the Device/s and set it/them to the Service-state? Then I can access all my devices manually per remote and update it by hand. I want to deploy new Apps through the Device Portal to safe time and have a effective administration. Also I wish there would be the possibility to do Batch- and Group-Deployments.
2. After I set the ctrlX CORE to Service-Mode, the download failed. We have access to the Test-Tenant since nearby 2 years, but didn't used it maybe now for about 7 - 8 months really. The last time we performed an update, it worked well. But now this Error happens:
[Here should be a picture, but the upload gives an error without a errornumber or helpful message, the attachment don't working too] So the message is: "Failed to install xxx-App Version x.x.x: InternalServerError: cannot perform the following tasks: - Download snap "..." (439 or 438) from channel ..."
The message isn't full readable (tooltip) and it is not possible to copy it. Something changed like addresses/FTP-Servers? Cause we use a proxy with a defined whitelist.
3. I tried to use the ctrlX Setup App and this didn't worked, but about this I'm in contact with a colleague of Bosch Rexroth. My point here would be, if the ctrlX Setup App works, it would be nice, if the configs could be loaded on the ctrlX COREs through the Device Portal.
Kind regards,
YourHighness