Hello community,
Is it possible to update code on safety controller remotely, e.g. via device manager, DOCKER or another way?
Reason for asking, is when a multiple number of machines are located around the world. It is then possible to update app, PLC and motion code etc with the device manager or using a service like DOCKER. It would then be nice to also remotely update the safety controller code instead of travelling and being onsite to do this.
Servodude
Remote update of safety controller
Best reply by CodeShepherd
A firmware update of the ctrlX SAFETY in the field remote is not possible. But started from FW 1.0.1.45, a SAFEX-C.1x can be updated via µSDcard. To update to 1.0.1.45 from former versions please contact your responsible Bosch Rexroth technician for further steps.
For HW exchange of a SAFEX-C.1x in the field, the safety program can be transferred to a new SAFEX-C.1x with µSDcard very easy.
After exchange of a safety control the machine has to be checked of all safety functions and has to be reported from the “service personal” which changed the SAFEX.-C.1x.
Also an update of the safety program via EoE and remote is possible but changing the safety program leads to the needof recertification mentioned above.
1 reply