10/25/2024
HD Vision Systems | App | Sense & Vision

HD Vision Systems - LumiScan CamDriver

The LumiScan Camera Driver is a comprehensive image acquisition application. It runs a ctrlX OS device like ctrlX CORE and is configured and controlled by the ctrlX Data Layer. Accessible through any web browser, LumiScan CamDriver provides easy access to raw data and allows you to quickly adjust basic settings such as exposure time or pixel format.
The communication process in the application is based on the concept of a handshake, which allows greater flexibility in negotiating parameters that are acceptable to devices and systems at both ends of the communication channel.

Features

  • Supports Ethernet-enabled, GenICam standard compliant cameras.

  • Setup and control via ctrlX Data Layer.

The settings configuration can be edited with built-in website.

ctrlX OS Homepage


There is also a WebDAV configuration upload option if the user wants to upload their own settings.

WinSCP login page



 

Compatibilty

  • ctrlX OS Version 2.6

  • ctrlX OS Version 3.6

Latest version 2.0

  • Improved speed and reliability

  • Future-ready architecture for upcoming features

  • Multi-camera support

  • One license required per camera

  • Existing CamDriver v1 users can continue using their current version

  • Upgrade to CamDriver v2 to access the latest features and improvements

Prerequisites

  • Ethernet-enabled, GenICam compliant camera

  • ctrlX OS

Supported Camera Brands

LumiScan Cam Driver currently supports cameras from the following manufacturers: HD Vision Systems, IDS, Lucid Vision Labs, Basler, Balluff, Baumer, and Hikvision. In addition, the CamDriver can support other GenICam/GigE Vision compliant cameras.

Cameras from other manufacturers have not yet been tested. If your camera manufacturer is not listed above, please contact us.

Documentation

  • see app download

Support

đź”— HD Vision Systems Customer Service
📞 +49 (0)6221 6721905
đź“§ HD Vision Systems Customer Service 1)

Related Links 

Curious?

You can test many apps free of charge with a virtual control system provided by ctrlX WORKS.
Just download ctrlX WORKS and follow this How-to

[link-button type="light" text="TRY IT NOW" target="_blank" href="https://community.boschrexroth.com/ctrlx-os-store-apps-oc2pqqwn/post/ctrlx-works-xOJLFLUiK4NGm5H"]



The Company 

HD Vision Systems is a leading provider of industrial image processing and AI-based automation solutions. Our hardware-agnostic platform enables seamless integration across a wide range of cameras, sensors, robots, and industrial systems, giving customers maximum flexibility and future-proof scalability. By combining advanced machine vision software with strong partnerships across the automation ecosystem, we deliver tailored, high-performance solutions for quality inspection, process optimization, and intelligent manufacturing. Together with our technology partners, we help companies accelerate digital transformation and unlock the full potential of Industry 4.0.



1) Note on data protection
The email is sent directly to the partner company! This company is responsible for the processing of the data contained. Please read their data protection information before sending this email! Bosch Rexroth is not responsible for the use of the partner company's support.

Categories
Sense & Vision
Platform
ctrlX OS
Vendor
Partner Apps