LumiScan Calibration is an application that improves the accuracy of position and orientation information for objects found in the scene by scanning a mapping provided as a TIFF file.
Simply said, LumiScan Calibration is used to transform the image coordinates into real-world coordinates. This enables the use of cameras in combination with robots for bin picking and object placement tasks.
LumiScan Calibration is installed from the App Store and configured via a settings file. It runs on ctrlX OS devices like ctrlX CORE and the user interface is ctrlX Data Layer.
The communication process in the application is based on the concept of a handshake, which allows greater flexibility in negotiating parameters that are acceptable to devices and systems at both ends of the communication channel.
Features
Setup and control via ctrlX Data Layer
Converts a point on a 2D image to a 3D point on a calibrated plane
The settings configuration can be edited with built-in website.
To use LumiScan Calibration, you must upload calibrated data as a TIFF file. Optionally, if you want to use your own settings, an application configuration upload is also possible.
Both can be done with WebDAV.
Compatibilty
ctrlX OS Version 2.6
ctrlX OS Version 3.6
Latest version 2.0
Improved speed and reliability
Future-ready architecture for upcoming features
Existing Calibration v1 users can continue using their current version
Upgrade to Calibration v2 to access the latest features and improvements
The app has been restructured to support future features.
Prerequisites
Calibrated data files. 2D to 3D mapping as a TIFF file provided by HD Vision Systems.
ctrlX OS
Documentation
see app storage
Support
🔗HD Vision Systems Customer Service
📞+49 (0)6221 6721905
📧 HD Vision Systems Customer Service 1)
Related Links
Curious?
You can test many apps free of charge with a virtual control system provided by ctrlX WORKS.
Just download ctrlX WORKS and follow this How-to
[link-button type="light" text="TRY IT NOW" target="_blank" href="https://community.boschrexroth.com/ctrlx-os-store-apps-oc2pqqwn/post/ctrlx-works-xOJLFLUiK4NGm5H"]
The Company
HD Vision Systems is a leading provider of industrial image processing and AI-based automation solutions. Our hardware-agnostic platform enables seamless integration across a wide range of cameras, sensors, robots, and industrial systems, giving customers maximum flexibility and future-proof scalability. By combining advanced machine vision software with strong partnerships across the automation ecosystem, we deliver tailored, high-performance solutions for quality inspection, process optimization, and intelligent manufacturing. Together with our technology partners, we help companies accelerate digital transformation and unlock the full potential of Industry 4.0.
1) Note on data protection
The email is sent directly to the partner company! This company is responsible for the processing of the data contained. Please read their data protection information before sending this email! Bosch Rexroth is not responsible for the use of the partner company's support.