LumiScan Annotation Framework is versatile software that allows you to annotate objects in an image, providing data for training and retraining neural network models used for a task such as object recognition or quality inspection.
The intuitive interface allows for any number of users, customization of the annotation settings, and an unlimited number of annotations.
LumiScan Annotation Framework provides seamless data exchange with other HD Vision Systems applications and doesn't require any AI knowledge.
Features
Allows multiple users.
Customization of the annotation settings, such as the thickness of the bounding box line.
Unlimited number of labels.
After each saved annotation, the LumiScan Annotation Framework also writes the following information to a JSON file:
• User name
• Unix timestamp
• Image name (PNG)
• Save file name (CSV)
The JSON file is saved in the raw directory under the name of the saved image.
Sequential comments are appended so you can track who made a change and when.
Prerequisites
Windows 10 or higher
Compatibility Notice:
Recent Windows updates KB5074105 and KB5077181 may cause compatibility issues with the encryption used in our Windows Engineering Apps.
If either of these updates is installed, users may experience issues when running the software. In this case, please try using a system without these updates installed or contact us for support.
Graphics Card: Minimum 16GB VRAM (24GB VRAM recommended, e.g., NVIDIA RTX 4080).
Purchase requirements
System Requirements: Requires a HD Vision Systems LumiScan Key (USB Dongle) - R911427110 XACC-0-USBVIS.
Licensing Model: One‑time Base License (R911423889) + Annual Subscription (R911423890), required both for operation.
LumiScan Key and both One‑time Base License and Annual Subscription license must all be valid to operate this app.
Component
Material Number
Purchase Type
Year 1
Year 2
Year 3 …
LumiScan Key
USB dongle
R911427110 XACC-0-USBVIS
One-time Purchase
✓
already owned
already owned
One-time Base License
Initial purchase
R911423889
One-time Purchase
✓
already owned
already owned
Annual subscription
Every year
R911423890
Annual Subscription
✓
✓
✓
Additional Notes
First‑year licensing setup: One‑time Base License (R911423889) plus 1‑year Annual Subscription (R911423890) are required.
Subsequent years licensing: Only the Annual Subscription (R911423890) needs to be renewed.
One HD Vision Systems LumiScan Key (USB Dongle) can be extended for additional products via configuration update of the dongle.
Order items via ctrlX Configurator: ctrlX Software → Accessories
Documentation
Support
ℹ️ HD Vision Systems Customer Service
☎️ +49 (0)6221 6721905
✉️ HD Vision Systems Customer Service 1)
Related Links
Curious?
You can test many apps free of charge with a virtual control system provided by ctrlX WORKS.
Just download ctrlX WORKS and follow this How-to
[link-button type="light" text="TRY IT NOW" target="_blank" href="https://community.boschrexroth.com/ctrlx-os-store-apps-oc2pqqwn/post/ctrlx-works-xOJLFLUiK4NGm5H"]
The Company
HD Vision Systems is a leading provider of industrial image processing and AI-based automation solutions. Our hardware-agnostic platform enables seamless integration across a wide range of cameras, sensors, robots, and industrial systems, giving customers maximum flexibility and future-proof scalability. By combining advanced machine vision software with strong partnerships across the automation ecosystem, we deliver tailored, high-performance solutions for quality inspection, process optimization, and intelligent manufacturing. Together with our technology partners, we help companies accelerate digital transformation and unlock the full potential of Industry 4.0.
1) Note on data protection
The email is sent directly to the partner company! This company is responsible for the processing of the data contained. Please read their data protection information before sending this email! Bosch Rexroth is not responsible for the use of the partner company's support.